<iframe src="//www.googletagmanager.com/ns.html?id=GTM-MZTJSD" height="0" width="0" style="display:none;visibility:hidden">
 

Tampa Convention Center / Tampa, FL / January 22-26 / Booth # 913

Featured Products

REVConnect

A Game-Changing Connectivity System

Belden designed a better RJ45 connectivity system: one that focuses on the needs of emerging applications, takes advantage of connectivity trends and addresses the pain points expressed by installers.

  • Reliable: REVConnect features a highly reliable termination for a secure, gas-tight connection proven to reduce rework at all category levels.

  • Easy: REVConnect's universal wiring manager supports all Category 5e, 6 and 6A cables with a single tool that covers the entire termination process, including cable preparation.

  • Versatile: The same universal core terminates a jack or plug. Field-terminable plugs, which support Category 6A and high PoE performance, can be terminated as quickly and easily as a jack.

REVConnect

Enterprise Closet "X" (ECX) Patch Panel Solution

Improving on Best in Class

Belden's new ECX platform is an elegant, flexible solution set that improves upon industry-leading patch panel solutions. The ECX platform is designed for LAN environments and provides an easy-to-deploy, efficient solution for installers.

The ECX platform complements the strength of Belden's existing FiberExpress Ultra High Density (UHD) platform within its data center portfolio.

ECX Fiber Patch Panel

Passive Optical LAN (POLAN)

High-Performance, Easy-To-Install and Scalable Solutions

POLAN systems can address scalability and flexibility issues often associated with traditional switch-based LAN environments, eliminating excess equipment and cabling.

Belden offers a complete POLAN passive solution set within the FiberExpress UHD portfolio, including passive optical splitters, fiber cable (composite copper/fiber cables), rack-mount/wall-mount patch panels and new all-dielectric armored fiber cable that provides small-diameter, superior protection for the fiber-to-the-ONT segment of your POLAN deployment.

POLAN

HDBaseT Solutions

4K Ultra High-Definition Multimedia Content Over One Cable

Based on results from our HDBaseT lab, Belden cables 2183P and 2183R were designed specifically for optimal performance in 4K HDBaseT transmission. These shielded cables deliver 4K content over 100 meters using a unique, small, sleek design. Combined with the new REVConnect plug, it is the easiest to install, most reliable HDBaseT cabling solution available!

HDBaseT Solutions

Ladder Rack Runways

Speed Up Deployment Time and Maximize Space

Ladder rack runways are effective, widely used cable management systems that support and deliver bundles of cable between cabinets, racks and closets, as well as along walls and suspended from ceilings. Belden's ladder rack runway systems speed up deployment time, maximize space, optimize cable bandwidth and provide maximum cabling density.

Ladder Rack Runway

FiberExpress (FX) Fusion

Splice-On Connectors

Splice-on connectors use fusion splicers to permanently join a fiber stub inside the connector with a fiber cable. The splice is protected within the boot of the connector, replacing the need for traditional pigtails because the splice is contained within the connector. The connector can be directly terminated using the patch panel's existing cable management features.

Technicians are embracing Belden FX Fusion for outside plant environments, data center installations and multi-dwelling unit (MDU) networks.

FX Fusion Splice-on Connectors

Small OD (28 AWG) Patch Cords

Belden offers Small OD Copper Patch Cords in Category 6 and Category 6A versions. Reducing congestion and improving airflow in cabinets, they are designed for data center applications. They also facilitate easier maintenance on high-density switches and allow better visual access to port labeling on patch panels. With the proliferation of IP devices in the networking infrastructure, the sharper bend radius of these patch cords allows connection in constrained areas.

Small OD Patch Cords

Events

Upcoming Events

Sunday, January 22 - Belden/Mohawk House Party

Click here for more info and to register!

Presentation Schedule

Lean Process Improvement - How to Positively Impact Your Projects and Business

  • Henry Franc, RCDD, OSP, CDCDP - Belden Canada, Mississauga, Ontario, Canada

1:30 - 4:30 PM

3 CECs

During this seminar we will explore process improvement techniques to help ICT users optimize their processes as they relate to ICT systems deployment. The seminar will also provide the ICT professional community with strategies and techniques to align their offerings with client needs. By working together and with collaborative goals, projects can be implemented more quickly, efficiently and with increased value to all involved. Using the example of data center deployment will provide real-world, concrete examples for participants.

Belden Breakfast Presentation @ BICSI

AVB: Don't Panic!

  • Don Parish

7:00 - 8:15 AM, Meeting Rooms 37 & 38

Simplified network infrastructure, reduced costs and support for next-generation AV applications are all possible with AVB (Audio Video Bridging). We will cover how AVB compares to other options for transporting audio and other real-time content over Ethernet as well as hints and tips on planning an AVB network.

Click here for more info and to register!

4k Cabling Truths and Misconceptions for HDBaseT

  • Bob Ferguson, RCDD, CTS - Belden, Indianapolis, Indiana, USA

8:30 - 9:15 AM

In a standards-based world, conflicting information about proper 4K cabling infrastructure leads to confusion and frustration. The HDBaseT signal has unique characteristics that are amplified with the increased bandwidth requirements of 4K. Using recent testing data from the Belden labs, attendees will learn the most important characteristics in four-pair cable used to support 4K HDBaseT and the idiosyncrasies of the conflicting messages in the market.