<img height="1" width="1" src="https://www.facebook.com/tr?id=1193025284112044&amp;ev=PageView &amp;noscript=1">

Cabling Performance and Next-Generation PoE


In this webinar:

With the forthcoming PoE++ Type 3 sending 49W of power to a network device, and PoE++ Type 4 sending 96W, the twisted-pair cabling infrastructure supporting that transmission will carry significantly higher wattages than ever before. With these higher power levels come new considerations such as heat rise and corresponding cable-bundle sizes.In the connectivity realm, the possibility of arcing or sparking upon unplugging of a PoE-powered device demands consideration.

This presentation discusses some of the real-world implications of deploying higher-wattage PoE on twisted-pair cabling. It pays particular attention to the physical and performance characteristics of cable and/or connectivity that affect the infrastructure’s ability to successfully deliver PoE.

Meet the presenter:

Stéphane Bourgeois is Director of Technology Strategy, Enterprise Networking, for Belden. Stephane holds a Bachelor’s Degree in Mechanical Engineering as well as a Master’s Degree in Science – Mechanical Engineering, from École Polytechnique de Montréal.

Throughout his 25-year career Stephane has worked in the telecommunications industry: He started his career with Nortel as a Design Engineer from 1989 to 1994, then as a Product Manager until 1999; from 1999 to 2007 he held various Sales and Marketing positions for companies such as ITF Optical Technologies, VoiceAge Corporation and had his own consulting company.

Stephane joined Belden in 2007 as Director Product Line Management, Enterprise Networking and since then has contributed to several product innovations including the 10GX Pre-Terminated Cabling System and the FiberExpress UHD System. Since 2014, Stephane as Director Technology Strategy is focusing on technology roadmap and ideation, networking applications and trends, and standards engagement.


Who Is Belden?

For more than 100 years, customers who have required unsurpassed performance and durability for signal transmission have counted on the Belden brand. In the 20th century, that trust was built on high-performance wire and cable products.

Today, Belden designs, manufactures and sells a comprehensive portfolio of cable, connectivity and networking products for the transmission of signals for data, sound and video applications.