<iframe src="//www.googletagmanager.com/ns.html?id=GTM-MZTJSD" height="0" width="0" style="display:none;visibility:hidden">
CP_KV_Kuwait-oil-pipeline

Case Study "Kuwait Oil Company"

This Case Study explains:CP_CS_116KuwaitOil

  • Why Hirschmann switches, Industrial HiVision Network Management System, and network technical support were chosen to develop a robust and reliable pipeline control network for Kuwait Oil Company. 

  • How companies like the Kuwait Oil Company operating long distance pipelines really benefit from the Industrial HiVision rapid fault location functionality.

This case study uncovers how Hirschmann successfully applied Hirschmann Ethernet technology to develop a robust and reliable pipeline control network.


From the Case Study:

"Administration and maintenance of the pipeline networks using Industrial HiVision is not only done quickly and efficiently, but also with minimized operational risk."
– Shariq Khan, Technical Manager, ZMS Technology

“The Fiber Optic Communication Network is based on Hirschmann Industrial Ethernet Switches, which are suitable for the harsh environment of Kuwait. These devices enabled us to deploy a fast, reliable and secured backbone network for transporting SCADA, various control signals, security and safety services for the Oil and Gas pipelines in KOC. Industrial HiVision network management system provides an efficient and effective means of configuring and supervising the Communication Network."
– Mohammad Al Ajmi, TPL Specialist –I, Kuwait Oil Company

 

Complete the form and download the Case Study